Other Parts Discussed in Thread: SK-AM68,
Hi,
I have integrated CAN data into the OOB demo for a custom board based on the IWR6843AOP. When I tested individual boards separately, it worked well. However, when testing more than one board simultaneously, usually only one worked correctly. It seems that the other boards encounter issues when trying to initiate data transmission in the presence of existing communication on the CAN bus. Occasionally, a board sends one message and then freezes.I'm attempting to analyze the problem. The network is short, and I've tested various terminal resistor setups. I'm using SK-AM68 to monitor bus traffic and have also checked traffic using a CAN analyzer and oscilloscope. All indications point to one device working well while the others are frozen.
Any ideas on what could be causing the problem?
Thank you,Adam