I have a question regarding the error in sensor sensitivity of DRV5055.
For the Z4 type, it is stated that when using a power supply of 3.3V, the sensitivity will be in the range of 7.1mV/mT (min) to 7.9mV/mT (max).
Does the stated error range include ratiometric error and sensitivity linearity error?
If the ratiometric error is maximum (±2.5%), is it possible to exceed 7.9mV/mT or fall below 7.1mVmT?