This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to make a wireless temperature sensor using CC1310 MCU. For the same I would
like to know which temperature sensors are most suitable to sense the temperature range of Electrical busbars
-40C to 125C is the range I need. Kindly suggest me the part number and if somebody help me to design the project I will appreciate and remain thankful.
I will use 433MHz frequemcy band. For the same, I need a transciever separately.
ISOTMP35 may be of interest for a bus bar. LMT84 may be appropriate in TO-92. If a PCB can be mounted on or near the bus bar, then any temp sensor in our portfolio would be acceptable. ti.com/temperature
thanks,
ren