Hello.
The bin file used was "long_range_people_det_6843_demo.bin".
Using the "mmWave Industrial Visualizer.exe" file provided by TI, the settings were set as follows to detect vehicles and people at intersections.
- Demo: Long Range People Detection
- Select Configuration: 6843_50m_3D.cfg
- Elevation Tilt: 2
- Sensor Height: 2
However, if the number of Statistics -> Points is more than 150, an error occurs that causes the GUI to stop.
The GUI seems to STOP if there is too much data being detected.
Is there any way to solve this?