Hello TI team,
We are using OPT3001 in Automotive HUD , but we are using opening angle of +/-12° , not +/-45° , I have some questions base on current design .
1: Can we improve the performance by software Compensate ? what the compensate value @ current design with +/-12° .
2: If we want to do some measurement to get the compensate value on bench or vehicle, then could you provide some suggestion . eg: How to create the test bench in details , what's the equipment we need , and so on ,
3:Currently , software setting the config 100ms automatic full scale , if any disadvantage to this mode compared to other fixed modes? Can we improve the photosensitive characteristics by other config setting by software ?
4:As i know the photosensitive characteristics depends on opening angle, transmittance, light source, light exposure angle, temperature, voltage, etc., we do not have vehicle test data about these lights and ALS.but we want to have quantitative empirical data for reference. IT should have a lot of professional test data and experience in considering different application scenarios. Can you share with us some other data and experiences that are not in the datasheet and are close to actual application scenarios?
Thanks