I am using SDK 05.03.00.02 and CCS 12.5.
I found that whether the IWRL6432Boost EVM is set in flashing mode or functional mode, the CCS debug functionality are available for execution after launching target configuration. Additionally, regardless of whether empty.debug.appimage/empty.release.appimage is flashed into meta image 1 by Uniflash or even if the entire flash memory is erased, the CCS debug functionality is still available. Is this normal?