Other Parts Discussed in Thread: IWR6843, AWR1843
Hi,
I have automotive toolbox folder "mmwave_automotive_toolbox_3_6_0__all". In this folder there is source code for medium range lab007 "lab0007_medium_range_radar". This source code I have used for AWR1843 to detect the object at long range up to 50m. Can I use the same code for IWR6843 just by changing the target in code composer studio or do we have different source code for IWR6843 for long range object detection up to 50m and if possible, more than 50m?
Thanks,
Manoj