1). mmwave studio configuration is as follows. Frame periodicity is 10ms. In a second it should have 100 frames and 200 frames in 2 seconds. But when i execute start frame, in the Raw_LogFile it shows the duration as 4 seconds.
2). Can i setup frame config in Infinite mode so the radar sensor transmit the frames infinitely but run dca1000evm data capture tool whenever i want to capture the data?