This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843: No result after sensor start

Part Number: AWR6843


Hi,

Currently, I try to start sensor without visualizer, I follow tie2e article to use bypass to start sensor.

https://e2echina.ti.com/blogs_/b/behindthewheel/posts/ti-mmwave-sensor

I adjust the CLI_open of cil.c in SDK.

int32_t CLI_open (CLI_Cfg* ptrCLICfg)
{
    Task_Params     taskParams;
    uint32_t        index;

    /* Sanity Check: Validate the arguments */
    if (ptrCLICfg == NULL)
        return -1;

    /* Initialize the CLI MCB: */
    memset ((void*)&gCLI, 0, sizeof(CLI_MCB));

    /* Copy over the configuration: */
    memcpy ((void *)&gCLI.cfg, (void *)ptrCLICfg, sizeof(CLI_Cfg));

    /* Cycle through and determine the number of supported CLI commands: */
    for (index = 0; index < CLI_MAX_CMD; index++)
    {
        /* Do we have a valid entry? */
        if (gCLI.cfg.tableEntry[index].cmd == NULL)
        {
            /* NO: This is the last entry */
            break;
        }
        else
        {
            /* YES: Increment the number of CLI commands */
            gCLI.numCLICommands = gCLI.numCLICommands + 1;
        }
    }

    /* Is the mmWave Extension enabled? */
    if (gCLI.cfg.enableMMWaveExtension == 1U)
    {
        /* YES: Initialize the CLI Extension: */
        if (CLI_MMWaveExtensionInit (ptrCLICfg) < 0)
            return -1;
    }

    /* Do we have a CLI Prompt specified?  */
    if (gCLI.cfg.cliPrompt == NULL)
        gCLI.cfg.cliPrompt = "CLI:/>";

    /* The CLI provides a help command by default:
     * - Since we are adding this at the end of the table; a user of this module can also
     *   override this to provide its own implementation. */
    gCLI.cfg.tableEntry[gCLI.numCLICommands].cmd           = "help";
    gCLI.cfg.tableEntry[gCLI.numCLICommands].helpString    = NULL;
    gCLI.cfg.tableEntry[gCLI.numCLICommands].cmdHandlerFxn = CLI_help;

    /* Increment the number of CLI commands: */
    gCLI.numCLICommands++;

    /* Initialize the task parameters and launch the CLI Task: */
   // Task_Params_init(&taskParams);
    //taskParams.priority  = gCLI.cfg.taskPriority;
    //taskParams.stackSize = 4*1024;
    //gCLI.cliTaskHandle = Task_create(MmwDemo_Bypass_CLI, &taskParams, NULL);
    return 0;
}

 Config setting: 1: 3D_People_Tracking  2: Overhead_3D_People_Tracking

 

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 60.75 30.00 25.00 59.10 657930 0 54.71 1 96 2950.00 2 1 36 
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 96 0 55.00 1 0
dynamicRACfarCfg -1 4 4 2 2 8 12 4 8 5.00 8.00 0.40 1 1
staticRACfarCfg -1 6 2 2 2 8 8 6 4 8.00 15.00 0.30 0 0
dynamicRangeAngleCfg -1 0.75 0.0010 1 0
dynamic2DAngleCfg -1 1.5 0.0300 1 0 1 0.30 0.85 8.00
staticRangeAngleCfg -1 0 8 8
antGeometry0 0 -1 -2 -3 -2 -3 -4 -5 -4 -5 -6 -7
antGeometry1 -1 -1 -1 -1 0 0 0 0 -1 -1 -1 -1
antPhaseRot 1 1 1 1 1 1 1 1 1 1 1 1
fovCfg -1 70.0 20.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
boundaryBox -4 4 0 8 0 3
sensorPosition 2 0 15
gatingParam 3 2 2 2 4
stateParam 3 3 12 500 5 6000
allocationParam 40 100 0.1 20 0.5 20
maxAcceleration 0.1 0.1 0.1
trackingCfg 1 2 800 30 46 96 55
presenceBoundaryBox -3 3 0.5 7.5 0 3
sensorStart
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 61.2 60.00 17.00 50 328965 0 55.27 1 64 2000.00 2 1 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 224 0 120.00 1 0
dynamicRACfarCfg -1 10 1 1 1 8 8 6 4 4.00 6.00 0.50 1 1
staticRACfarCfg -1 4 4 2 2 8 16 4 6 6.00 13.00 0.50 0 0
dynamicRangeAngleCfg -1 7.000 0.0010 2 0
dynamic2DAngleCfg -1 5 1 1 1.00 15.00 2
staticRangeAngleCfg -1 0 1 1
antGeometry0 0 0 0 0 -1 -1 -1 -1 -2 -2 -2 -2
antGeometry1 -3 -2 -1 0 -3 -2 -1 0 -3 -2 -1 0
antPhaseRot 1 1 1 1 1 1 1 1 1 1 1 1
fovCfg -1 64.0 64.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
staticBoundaryBox -3 3 -3 3 -0.5 3
boundaryBox -4 4 -4 4 -0.5 3
sensorPosition 2.9 0 90
gatingParam 3 2 2 3 4
stateParam 3 3 6 20 3 1000
allocationParam 20 20 0.05 20 1.5 20
maxAcceleration 1 0.1 1
trackingCfg 1 4 800 20 37 33 120 1
presenceBoundaryBox -4 4 -4 4 0.5 2.5
sensorStart

The Overhead_3D_People_Tracking in RadarTool_Box can successfully start sensor with bypass manner and PC can receive data, the 3D_People_Tracking in RadarTool_box can start sensor but no data is sent to PC.I think that DSS core does not perform Pcount3DDemo_DPC_RadarProc_dpmTask,because Pcount3DDemo_DPC_RadarProc_reportFxn has not been performed after starting.

Regards,

Nick. 

  • Hey Nick,

    Thanks for reaching out regarding CLI bypass. Have you verified that the application runs the MmwDemo_uartTxTask and has valid data to write over UART? Are there any errors reported in the console, and if so, what are they? Have you tried following the Hard Coded Config User Guide in the Radar Toolbox instead? The E2E article you linked is based largely off of the Radar Toolbox guide and offers a slightly different approach that does remove the CLI task which could be disrupting task priority.

    Regards,

    Kristien