We will use 2 pcs TMP451 with one I2C bus on board, but the I2C slave address can't be changed, fixed on 4CH.
How to modify the I2C slave address or could you have any suggestion?
tks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We will use 2 pcs TMP451 with one I2C bus on board, but the I2C slave address can't be changed, fixed on 4CH.
How to modify the I2C slave address or could you have any suggestion?
tks.
Hi Vicky,
The TMP451 comes in 1 address only. TI may be able to produce it with a different address if the business case is large enough. Otherwise, you would have to use an I2C switch/MUX to communicate with multiple devices of the same address on the same bus. I would also recommend looking into the TMP451-Q1 which is SW compatible and features the following addresses:

Best regards,
Simon Rojas