This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5170-Q1: zero position confirmation for different batches

Part Number: TMAG5170-Q1

Dear,

 One customer need to confirm about the TMAG5170-Q1, since each product is different according to the position error and magnet filling error will cause the magnetic sensitivity of the HAL , how should we define the zero position for different individual products?

Best regards

kailyn

  • Hello Kailyn, 

    When you say zero position, what does that refer to? Is it a rotational or linear motion? 

    If possible, they could perform a calibration measurement with the TMAG5170-Q1 after assembly to determine the magnet position and use that as an offset for the zero position. 

    Best Regards, 

    Justin Beigel