Other Parts Discussed in Thread: OPT3101
Hi Team!
What is the maximum distance that the OPT3101 EVM hardware can measure?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team!
What is the maximum distance that the OPT3101 EVM hardware can measure?
Hi Pengsheng,
The EVM can measure up to 15 m distance.
Thank you,
Brent Elliott
Brent:
What is the Field of view (FOV) of the OPT3101 EVM transmitting tube and receiving tube respectively?
Thanks
Pengsheng,
The field of view of the photodiode is 10 degrees half angle. In practice the tube will block the IR emitter from hitting the photodiode directly, which means that the height of the tube should never interfere with the angle of the IR beam. A narrower beam will mean longer distance, as a wider beam will reduce the distance to increase the width.