Other Parts Discussed in Thread: AWR1843
hi,
when I use AWR1843boost to collect the raw data of one object, so that I can estimate the object's Azimuth Angle.
I set one tx antenna enable and four rx antennas enable. and I know the angular resolution formular is: lambda/(Mdcos(theta)), here, M= 4 for my settings in AWR1843.
based the formular when M=4, when the actual angle is 0 degree, then angular resolution is about 28.6 degree.
when the actual angle is 30 degree, the angular resolution is about 33 degree.
my question is:
according to the angular resolution formular, I found another formular about angular accuracy:

so I want to know using awr1843 to detect object and estimate the angle, what value is the angular accuracy generally? give me some cases in number, thank you.
Regards,
Wembanyama