Other Parts Discussed in Thread: HDC3020, HDC1010
I have two questions about this product (HDC1000). The first one is regarding the electrical characteristics, the second about the long term drift effects. I've already contacted customer support but they suggested to post a forum question so here we are. I hope one of you can help me with this.
In the datasheet the following point is written down: (7) Recommended humidity operating range is 20% to 60% RH. Prolonged operation outside this range may result in a measurement offset. The measurement offset will decrease after operating the sensor in this recommended operating range.
Would someone be able to more accurately define prolonged? What should I think of this? What would be the "negative" effects after 1 minute above 60%RH, and what for 1 hour, 1 day, 1 week, 1 month, 1 year. And what period do I need to think of when I read "offset will decrease after operating the sensor in this recommended operating range"? Does it behave proportionally with the definition of prolonged? For example, 1 day above 60% creates an offset, and it needs another day to recover?
The second question is about the long-term drift. On the datasheet, it says long-term drift is 0,5%/Year, Under which conditions does this happen? and does it drift faster if the product operates in an environment where the RH is between 40-80% with peaks of 95%? In that case what %/Y would I more likely have? Would I be able to get an estimation?
Links to the product:
HDC1000 data sheet, product information and support | TI.com