Other Parts Discussed in Thread: AWR6843
When we evaluate our AWR6432 module, sometime the noise level is drastically rising up. And it depands on the module design.
Seeing range profile of each antenna, the module waht the DC leak level is higher would be that the noise level is also higher.
The DC leak level of TI EVM is lower and the there is also no noise increasing.
We also tried to control the Rx gain, HPF norner and Tx Backoff. If we change the each value to suppress the DC leak level (that means Rx Gain lower, HPF corner is higher, Tx Back-off is larger), the noise increase is disappered.
And this phenomenon is not observed about AWR6843 module evaluation.
So then, should we supress the DC leak enough when we use AWR6432 module?
And if you know would you tell something about the relationship between DC leak and noise increase?
This is the range profile result of our module and TI EVM. (FW is our original based on Motion and Presence from SDK5.3)
This evaluation was conducted in chamber box. We are thinking that the peak around 50cm would be the reflection from inner wall of chamber.
・TI EVM
・Our module
Thank you,
Best regards
Tak