Other Parts Discussed in Thread: IWRL6432, IWR6843ISK, DCA1000EVM
Hello,
I wanted to capture the RAW ADC data from IWRL6432Boost using DCA1000 via ethernet using CLI application(I'm using presence and motion detection code demo example).
SDK: MMwave_L_SDK_05_03_00_02
MMwave_studio_04_01_00_01 for CLI Commands
Flashed EVM with Presence and Motion detection at Flash Mode. Followed Iwrl6432 for Switch settings
Made changes in config file with ADc data logging 1, low power cfg 0 for DCA data capture
Change Switch settings to Debug/DCA mode and connected the DCA
Below shared the results of CLI_log file i have received the success messages for every command sent. However i get a NO LVDS information at last. Unable to capture the data. Can you please guide how to resolve this. Thanks
Thu Jan 11 11:10:06 2024
FPGA Configuration Command (req)
Thu Jan 11 11:10:06 2024
FPGA Configuration command : Success
Thu Jan 11 11:10:06 2024
Return status : 0
Thu Jan 11 11:10:14 2024
Configure Record Command (req)
Thu Jan 11 11:10:14 2024
Configure Record command : Success
Thu Jan 11 11:10:14 2024
Return status : 0
Thu Jan 11 11:10:23 2024
Start Record Command (req)
Thu Jan 11 11:10:23 2024
Start Record Command (req)
Thu Jan 11 11:10:23 2024
Start Record command : Success
Thu Jan 11 11:10:23 2024
Return status : 0
Thu Jan 11 11:10:23 2024
Start Record command : Success
Thu Jan 11 11:10:53 2024
No LVDS data
Thu Jan 11 11:10:53 2024
Record stop is done successfully