Can I use LDC1314 with a target that is made from 1018 or 1045 Carbon Steel (and it is magnetic)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use LDC1314 with a target that is made from 1018 or 1045 Carbon Steel (and it is magnetic)?
Hi Eugene,
Yes, the LDC1314 can be used with carbon steel if the frequency is high enough. Typically, the frequency will need to be >300kHz.