This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOPEVM: mmWave Demo visualizer invalid configuration

Part Number: AWR6843AOPEVM

Hi Ti,

I got some problem when I using mmWave Demo visualizer。
I want to change the parameter inside the cfg.,but after I revised it shows me "Invaild configuration"

When I use this cfg.
mmWave Demo visualizer can work.

      

I changed "profileCfg 0 60 7 3 24 0 0 166 1 256 12500 0 0 158" into  "profileCfg 0 60 7 3 24 0 0 150 1 256 12500 0 0 158"
mmWave Demo visualizer can't work, and showed "invalid configuration"

  


I have also tried changing other parameters, but "invalid configuration" always appears. Please help me clarify the reason.
I hope to use different parameters for calibration and experimentation.

Thanks
Vincent