Other Parts Discussed in Thread: OPT3004
Hello Expert,
Our customer have a plan to use this device.
There are specifications I would like to check before final application.
I would appreciate it if you could reply to each item.
1) Based on 6500K color temperature, is there Photo Current data for each Lux?
2) There doesn't seem to be an exact value for Angle of Half Sensitivity in the datasheet. Can I see it as (typ) 58º on the graph?

3) We request the min and max values of the Sensitivity Wavelength Range. The datasheet only lists Peak=550nm.

4) Does the “OPT3005” product have a built-in temperature compensation circuit?
5) We compared the Normalized Response data according to temperature of “OPT3004” and “OPT3005”.
If a temperature compensation circuit exists in the “OPT3005” product, can it be said that its performance is lower than that of the “OPT3004”?

6) Is there any graph data showing Dark Current compared to Temp?
Best Regards,
Michael