Other Parts Discussed in Thread: LDC1101, LDC0851,
Hi team,
Can our inductive sensor recognize metal materials differences?
I've seen material target graph which might recognize the materials on Figure 2-1 with below link.
https://www.ti.com/lit/an/snoaa76/snoaa76.pdf
Customer application is induction range and they want to recognize like AL1100, Steal and Stainless steel.
Target distance from the pot coil is fixed (4~6mm) and target area is large enough (over 100mm radial).
If we could, then which device could be the best? (LDC3114, LDC211x, LDC161x, LDC0851 and LDC1101)
Or if we can't, then would you roughly explain the reason?
Best,
Ernest