Hi,
If we modify FOV of azimuth and elevation, then will it effect on range of radar.
For e.g.
Azimuth -90 to 90 degrees
Elevation -90 to 90 degrees
Range 59.99m
Doppler -30 to 30
Above configuration is as per 50m 2d LRPD config.
So, if I change azimuth to -40 to 40 degrees then this will affect the range of 59.99m? If yes then how this effect will take place whether range will increase or decrease?
Thanks,
Manoj