This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001-Q1: Measurement output variation

Part Number: OPT3001-Q1


Hi team,

My customer have questions about OPT3001-Q1 output variation.

・ The following variation in measurement output is approximately +/- 10%. Is the variation from the initial tolerance?

・ In addition, what is the measurement output variation based on the actual value?

・ In datasheet, it is described variation when Full-Scale Range:2620.80Lux, LSB Size: 0.64. Could you tell me how to estimate the customers situation.

They want to estimate when Full-Scale Range:40.95Lux, LSB Size: 0.01.

Regards,

Youhei MIYAOKA