Hello
I have a question about the current consumption of DRV5055A2QLPGM.
The current consumption is 6 to 10 mA in the data sheet before December 2023.
The data sheet was revised in December 2023, and the current consumption has been changed to 3 to 5 mA.
When I applied a voltage of 5V to the DRV5055A2QLPGM that I obtained, the current consumption was 7mA.
"3CVOWF" and "55A2" were printed on the surface of the DRV5055A2 I obtained.
Is the DRV5055A2 I got an old datasheet?
Are there any changes to the product along with the datasheet changes?