Other Parts Discussed in Thread: AWR2944
Hi,
Can any one tell me the differences betweent the two chips,from these aspects,such as the max measure range, azimuth resolution,elevation angle resolution, the number of cloudpoint etc;
BR
Rata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rata,
Here are some high-level thoughts regarding your question:
Combining the points above, you should be able to determine the capabilities of the system for your use case.
Regards,
Kaushik
Hi Kaushik,
Thanks for your reply. Now AWR2544LOP EVM can be provided. If I use this demo board, is the performace better or worse than AWR2944 EVM in the aspects,such as the max measure range, azimuth resolution, elevation angle resolution, the number of cloudpoint etc?
For example the max range is up to 200m for the AWR2944 EVM, the azimuth resolution is 9.5°, the azimuth field of view ±80º and so on. Whether are the level parameters almostly similar about the two boards? Because the two EVMs are both 4 receive and 4 transmit channels, the TX power ,phase noise and Rx noise figure parameter are similar. What is the level parameters of AWR2544LOP EVM?
BR
Rata
Hi Rata,
It appears that my point has not come across clearly and there is still some confusion. System level parameters such as the max range, max velocity, range and velocity resolution, and number of point cloud are heavily dependent on the processing capabilities of the device.
For example, If there is more memory and processing capabilities, you can have a larger number of DDM sub-bands. more number of samples, larger cube, higher resolution FFT and more advanced angle estimation algorithms such as MUSIC etc. On the 2544, only the range processing is done on the SoC and the 1D FFT data (compressed) is sent out to a central processor. There are also multiple AWR2544 devices intended for use around the car in a satellite architecture whose data will be combined and processed together. This can significantly alter parameters like angular resolution, field of view in azimuth etc.
In a single device to device comparison, what the AWR2944 and the AWR2544 output will be different. That is to say, the AWR2944 device provides a point cloud or an object list whereas the AWR2544 outputs the full 1D Radar cube. (You can also refer to our demos for this)
Regards,
Kaushik
Hi Kaushik,
Thanks for your detailed reply.May be my expressiong is not clear.
As you said, the max range, max velocity, range and velocity resolution are heavily dependent on the processing capabilities of the device such as memory or processing capabilites ,or algorithm. It is very reasonable.Now we do not consider these factors, we view this problem in the physical level.
Now only considering the antenna itself , we take the max range Rmax as an example. The formula can be expressed as belows:
Here, Rmax is the physical limit max range. From this formula, if AWR2944 Rmax is same with AWR2544,can I say that the two EVMs deliver the same performace?
Another is azimuth resolution, if super resolution algorithm is introduced, the angle resolution can be improved,but it is suitable for both AWR2944 and AWR2544.Now without considering the super resolution algrithm, the azimuth resolution is decided by the number of Tx and RX antennas.In this level, can I say the resolution are idential for AWR2944 and AWR2544.
BR
Rata
Hi Rata,
With respect to the front-end only capabilities, the performance of the AWR2544 would be very similar to that of the AWR2944. The main difference comes with the SNR improvement with the LOP packaging of the device. This makes it such that farther objects can be distinctly detected instead of being buried in the noise floor.
Regards,
Kaushik
Hi Kaushik,
Thanks for for your reply, I got it. I have another problem, you said ' The main difference comes with the SNR improvement with the LOP packaging of the device.', why is SNR improved with the LOP packaging of the AWR2544LOP EVM?Or which parameter can illustrate this point?
BR
Rata
Hi Rata,
Recommend you go through this document for an insight on LOP technology,
Advancements in mmWave Technology: Launch on Package for Automotive Radars
Regards,
Kaushik