This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6243: OSC_CLOCKOUT level

Part Number: IWR6243
Other Parts Discussed in Thread: AWR2243

When the component is run in cascade mode the slave(s) will receive a clock on the CLKP pin from OSC_CLKOUT via a DC-block. The level of this clock is measured to be 1.35V p-p, significantly higher than the specified max 1200mV on the CLKP input. Is this ok?

Related to this similar thread on AWR2243?

AWR2243: The OSC_CLKOUT signal output range more than 1.3V