Hi, I had a couple of questions. I was wondering if someone could check and verify my design/ layout? Want to make sure the SHLD connections as well as the traces in parallel with the CIN traces make sense. Also, my next question is about trace lengths connected to the CINn inputs. Does it need to be matched? For example, the length of my CIN1 trace from the FDC1004 pad to a connector is 35.63mm vs for CIN3 the trace length is only 16.9mm. Will this present issues when the measurement is taken? I plan to do a differential measurement. Any feedback would be much appreciated.
Thanks!SENSOR_BOARD.zip