This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Modify, compile and flash default firmware to enable SYNC_IN pin for triggered mode

Part Number: AWR1843BOOST

Hello,

We are working on a project that requires synchronization between a camera and the AWR1843BOOST board. We would like to use the SYNC_IN pin so that we can send a pulse to trigger the radar to send frames at a specified time. How is the default firmware modified to enable the SYNC_IN pin and which program can be used to compile and flash the firmware back onto the AWR1843BOOST board. Does the trigger pulse have any special requirements?

Thks

Mark