Hello,
As per the errata of AWRL6432, maximum baud rate for UART is 115200 bps, could you please let us know of any workarounds that can be done to use higher, standard baud rates for UART?
Thanks,
Sowmya N
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
As per the errata of AWRL6432, maximum baud rate for UART is 115200 bps, could you please let us know of any workarounds that can be done to use higher, standard baud rates for UART?
Thanks,
Sowmya N
Hey Sowmya,
As mentioned in the meeting today, you can test out 500 kbps to see if it works, but we have also tested 1.25 Mbps and confirmed that it works with infrequent bit errors. Unfortunately, there is no way of achieving a standard baud rate higher than 115200 bps.
Let me know if 500 kbps or 1.25 Mbps does not work or if you need help with anything else.
Regards,
Kristien