This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: IWR1843Boost

Part Number: IWR1843BOOST

Hi,

I succeeded to setup and connect the EVB IWR1843Boost with my PC with the TI dev cloud.

What is the right way to:

1. Set Real and Imaginary data for each Tx channel from the EVB?

2. Record into my PC the Real and Imaginary data from each Rx channel from the EVB?

Best regards,

Shai

  • HI Shai,

    If you're looking to record the raw time-domain ADC data from the radar device, then you will need the DCA1000 capture device. With the IWR1843BOOST board, you can extract point cloud data, but IWR1843BOOST by itself cannot stream the raw adc data to the computer - the data rate is too fast.

    Best,

    Nate