This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: when adding IPC RPMessgae Function,it will come out this situations.

Part Number: AWR2944


Hi  TI Support,

      when building CCS project,it will report this error,like as ,"../linker.cmd", line 106: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".bss.ipc_vring_mem" size 0x1ec0. Available memory ranges:
RTOS_NORTOS_IPC_SHM_MEM size: 0x1d40 unused: 0x1d40 max hole: 0x1d40  

      when adding IPC RPMessgae Function,it will come out this situations.

     Cheyrl.wang

  • Hi Cheryl,

    Can you please state your question clearly?

    Please provide some additional details on this so that we can proceed further - 

    * What project are you exactly trying to build and run?
    * Which CCS version you are using?
    * What device you are using?
    * What is the exact issue?
    * What is IPC RPMessage here? How are you trying to include in your code?

    Thanks,
    Anirban