I am using the mmWave Demo Visualizer to carry out the evaluation.
The diagram below shows the graph when the module is placed against a wall.
I understand that if the difference between the Noise Profile and Range Profile peaks is greater than the CFGR threshold, it is plotted as Detected Points, is this correct?
For example, the red circle in the diagram below is not plotted as Detected Points even though its peak is larger than the blue circle.
Why is this, and is it related to the distance as well as the peak value of the Range Profile?
Best Regards,