Hi,
I would like to ask about position information.
・Where are the posX, posY, and posZ in the Target List TLV based on? Where is (0,0,0)?
・Also, is it correct to recognize that the position data indicates the position of a person's chest?
・Is it possible to obtain angle and distance information between the sensor and the person?
[Environment]
▼Sample App Version
rader-toolbox 1.30.01.03 mmWave Industrial Visualizer
「Vital Signs With People Tracking」
▼OS Version
Windows 10Pro 22H2
▼ Driver version information recognized by Windows side
XDS110 Class Application/User UART version 2.0.0.2
XDS110 Class Auxiliary Data Port Version 2.0.0.2
Best Regards,