Part Number: DRV5032
We are using a North facing magnet inside pump head to be able to detect the rotation speed(RPM). The magnet sits12.5mm away from the DRV5032FDDMR when it passes on top of it. The magnet is spec to have a min of 55mT(We dont have the specifics of the magnet). When we see the output of the DRV5032, we see the it is inverted. Is low for about 50 to 100mS and then high. The datasheet states that this is possible
When the applied magnetic flux density exceeds the BOP
threshold, the device outputs a low voltage. The
output stays low until the flux density decreases to
less than BRP, and then the output either drives a
high voltage or becomes high impedance, depending
on the device version.
What is not understood is whether this is OK to have. We recently just started seeing that the device misses pulses and our system faults when this happens. If this is not advisable, any idea what needs to change to make this work reliably.
Thank you for your help.