I have two questions regarding the OPT3101 register.
opt3101 datasheet
・About his FREQ_COUNT_REG at register address 11h
What are the conditions that change the value of this register?
- Read the register from 1h to b9h.
The value of "RESERVED" in "Register 5h" changes every time I perform a measurement.What is the reason for this change? What does “RESERVED” here mean?
For example:
1st time 5h:808c0
2nd time 5h:808c8
Why? ?