Other Parts Discussed in Thread: DCA1000EVM, IWR6843AOP, MMWAVEICBOOST, , IWR6843
I have just acquired the IWR6843AOP and a DCA1000EVM. I initially want to start with raw data collection. The two boards are connected properly. First, my PC does not have an ethernet port, so I am using an ethernet to USB adapter. I think it is working. I have loaded the mmWave_studio, and have the ethernet and USB J1 on the DCA1000 both connected. One of my USB drivers seems to be correct seeing four(4) instances of the AR-Dev-Pac-EVMs on the com ports and USB. However, the USBs called XDS-110 Class Application/User UART and XDS-110 Class Aux Data Port are not seen (only USB composite devices). Where is that driver? Also, when running mmWave_studio, the BSS and MSS packages are not found. Where can I download these for the 6843 in mmWave_studio Connection window? Please advise. Thanks!