Other Parts Discussed in Thread: IWRL6432, UNIFLASH
SDK: 05_03_00_02
demo example: MCan external read write demo
I'm trying to run example code Mcan external read write demo on IWRL6432. However i don't see anything on the Pcan view.
Here are steps i have followed please let me know if i have missed anything:
Flashed MCan external read write demo using UniFlash
Flash Mode switch settings :
S1.1 --> OFF
S1.2 --> OFF
Flash was successfull
Changed to Functional Mode and reset the h/w. Below are the switch settings made using the reference information provided in the document:
S1.1 --> ON
S1.2 --> OFF
S1.3 --> OFF
S1.4 --> OFF
S1.5 --> OFF (CAN)
S1.6 --> OFF
S4.1 --> OFF
S4.2 --> OFF ( CAN PHY : Standby Mode Disable) as mentioned from the reference document
S4.3 --> OFF
file:///C:/ti/MMWAVE_L_SDK_05_03_00_02/docs/api_guide_xwrL64xx/EXAMPLES_DRIVERS_MCAN_EXTERNAL_READ_WRITE.html
On the UART Terminal i was able to see the message application started. However i was not able to see any outptut on PCAN View:
Peak CAN pins:
CAN L --> pin 2
GND --> pin 3
CAN H --> pin 7
After all the above settings i do not see any CAN message on Receive window in PCAN View. Please let me know if i have missed out any steps to perform. Thanks