Hi E2E,
Good day.
Here is my application of LM335. And the block diagram is shown below.

I give 5V from PCB to LM335, and use MCU to sample the output voltage of LM335, then convert the voltage to corresponding temperature.
Then I put the whole set into a chamber to test it under different temperature condition.
In the beginning, the data show well and stable. However, when I change the environmental temperature in the chamber, the data fluctuate dramatically and could not recover.
So I want to inquire could TI provide me some internal test data of LM335 like the output voltage response in the period of temperature change.
I want to clarify the LM335 is able to work well in the range(−55°C to 150°C).
Thanks a lot!