Hi,
We are testing Evaluation board FDC1004EVM to measure small capacitances.
We have an important constraint about the good stability of capacitive offset in the time and with temperature.
Our goal is to measure small capacitance (for example 1pF) with a few fF error on temperature range from -20°C to 85°C.
We tested Evaluation board from 24°C to 44°C and 24°C to 84°C temperature range.
We tested the chip in single-ended mode and differential mode.
We get a good offset drift when there is no capacitance between CIN and SHLD.
But when we add a capacitance between CIN and SHLD (10pF or more) on one CIN channel or all channels, we observe a strong jump (5fF to 50fF) on all channels. These jumps appear at a temperature close to 40°C.
When temperature returns under 40°C, the offset errors becomes good again..
Could you please give us a first comment about these behaviors?
Are there specific parameters on this chip to improve offset stability in comparison with our results?
Thank in advance for your help.
Best regards
Didier