Other Parts Discussed in Thread: AWR6843AOP, AWRL6432
Hi, There
i want to know very basic radar knowledge.
here is our test environment.
1. position a test object which is occur same Doppler during operation.
2. there are two radar sensor (AWRL6432 / AWR6843AOP ) . and then measure max doppler value on each radar.
[Result]
- AWRL6432 radar detects Doppler value consistently.
- but, AWR6843AOP radar don't measure Doppler value consistently.
So, i really know which reason make a difference like this.
AWRL6432 : BPM (Binary phase modulation) , ADC sample more big than 64 , 2tx,3rx
AWR6843AOP : TDM(Time division multiplexing) , ADC sample 64 , 3tx 4rx
The first thought that comes to mind ,
AWRL6432 has more big adc sample, Thus can detect very high resolution value
however AWR6843AOP can miss max doppler value.
is it right opinion?
please your radar knowledge.