This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: Azimuth and Elevation Field of View

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: TIDEP-01012,

Hello,

I am trying to find out what the field of view is for the MMWCAS-RF-EVM, from the design guide (TIDEP-01012) it is stated that antenna field of view is +/- 70 deg. Is this just for azimuth plane? This would seem to match up with the antenna pattern plots which show 3dB bandwidth of ~70 deg across the tx and rx arrays.

Also, what is the unambiguous field of view in both the azimuth and elevation planes? (assuming MIMO and not beamforming operation)

And what is the antenna field of view in the elevation plane as the antenna pattern plots would suggest that it is only +/-20 deg.

TIA,

Alex