Part Number: AWR2243
Hi,
In AWR2243 cascaded system, slave devices use external frame syn signal for frame trigger and this frame sync signal will route back to host. There is frame trigger delay after sync in pulse input to real frame start (chirp transmit). What is the range of frame trigger delay time across different AWR2243 devices?
Customer asked this question is that they plan to change phase shifter in each TX/chirp. They concerned that if there is a big difference on the frame trigger delay in different devices it will affect the ADC data and the detection result.
Would you pls help? As the phase shifter accuracy on AWR2243 is ±5C, may the small different delay time not affect the result much?
Thanks,
Chris