Other Parts Discussed in Thread: , MMWAVEICBOOST, UNIFLASH
Hello,
I have two boards that use the IWR6843 device. One is an IWR6843ISK Rev B attached to an MMWAVEICBOOST board, and another is a Mistral board. I can not get code I built from examples to run on either.
I am currently trying to run binaries built for the Long_Range People_Det_6843 example. There have been no modifications to the project, and I am using CCS 12.6.0.00008 on a Windows 11 machine.
I built the binaries as release on the DSS version of the project. The binaries build without error, but when I use UniFlash to load the binary into the, I get the error ".... indicates it is not a valid file to flash to IWR6843"
I have also tried building the project as MSS in debug mode to run on the MMWAVEICBOOST in combination with the IWR6843ISK Rev B. Again, the code builds without errors, but the debugger fails to load. In CCS I get the error "XDS1110 USB ...." "Error initializing emulator: (Error -260 @ 0x0)"
I can load the prebuild binaries for the long-range people detector onto the Mistral, and it works with the "mmWave_Industrial_Visualizer" when I load a chirp file, but that's all the functionality that I have currently.
Any help with these issues would be apprishated.
-Tom