This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Effect of configuration files on diffuse reflection

Part Number: IWR6843ISK


Hi 

Using the configuration made by the "mmwave sensing estimator" causes a lot of object diffuse reflection.

In this way, the X axis deviates a lot from the center.

Using the 70m config provided by the "traffic monitoring lab", there is almost no reflex.

I don't know the correct configuration value. please help me.. 

Is there a problem with the configuration I'm using?

The test environment goes back and forth between medium-sized SUVs.

The following is my configuration file

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 63.5 2 3.8 21.74 0 0 7.5 1 211 12500 0 0 30
chirpCfg 0 0 0 0 0 0 0 4
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 64 0 50 1 0
lowPower 0 0
guiMonitor -1 0 1 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 9 0
cfarCfg -1 1 0 4 2 3 1 11 0
multiObjBeamForming -1 1 0.5
clutterRemoval -1 1
calibDcRangeSig -1 1 -5 8 256
extendedMaxVelocity -1 1
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 4 63 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -45 45 -90 90
cfarFovCfg -1 0 0 200
cfarFovCfg -1 1 -30 30.00
staticBoundaryBox -20 20 10 290 -0.5 3
boundaryBox -25 25 10 300 -0.5 3
gatingParam 12 8 5 5 0
stateParam 15 10 10 1000 10 1000
allocationParam 60 60 1 4 8 2
maxAcceleration 50 50 0.1
trackingCfg 1 2 250 20 113 355 50
sensorPosition 0 0 6
presenceBoundaryBox -3 3 2 6 0.5 2.5
sensorStart
Divide chirpCfg by 1 and 4 and it makes me more reflective.

Is there any good way to solve my reflexes?
I think "profileCfg" made by "estimator" is a problem.
Thank you for accepting my question
regards
Kim