This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART setup for connnecting CC1352 to PC

Other Parts Discussed in Thread: SYSCONFIG

I want to set up UART to send pixel data with UART. My device is CC1352. In arduino, this is made like this:

    //enable serial
  UBRR0H = 0;
  UBRR0L = 1;//0 = 2M baud rate. 1 = 1M baud. 3 = 0.5M. 7 = 250k 207 is 9600 baud rate.
  UCSR0A |= 2;//double speed aysnc
  UCSR0B = (1 << RXEN0) | (1 << TXEN0);//Enable receiver and transmitter
  UCSR0C = 6;//async 1 stop bit 8bit char no parity bits

I wrote it like this:

// UART Setup
UART2_Handle uartHandle;
UART2_Params uartParams;
UART2_Params_init(&uartParams);
uartParams.baudRate = 1000000; // 1M baud rate
uartHandle = UART2_open(CONFIG_UART0, &uartParams); // Replace CC1352_UART_INSTANCE with actual UART instance

What should I write to CONFIG_UART0? It is written in its documentation in the same way.https://software-dl.ti.com/simplelink/esd/simplelink_cc13x2_26x2_sdk/4.20.00.35/exports/docs/tidrivers/doxygen/html/_u_a_r_t2_8h.html

Also, I want to send pixel data to my PC to show the image. In arduino:

UDR0 = (PINC & 15) | (PIND & 240);
How can I send "uint8_t pixelData" to my PC with UART, or are there any other way?

Your help would be appreciated.