This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1815: LM1815

Part Number: LM1815


Hi Team,

As we are using this chip in our design, We need some Technical clarification.

1.In the datasheet Page 2, electrical characteristic data is provided for VCC 10V typical.

Can you please provide the electrical characteristic data for the VCC 3.3V and the 5V.?

2. If point 1 can not be provided then considering the following data,

 a. Input signal at pin 3 is between +12V and -12V sinusoidal,

 b.  Vcc

Case 1. 3.3V and  Case 2. 5V

Kindly provide,

a. Output voltage levels for the Vcc 3.3V and 5V as well.

b. Arming Voltage level For the Vcc 3.3V and 5V as well.

3. Figure 17. LM1815 Adaptive Sense Amplifier is for the VSIGNAL is a Sine Wave; FSIGNAL is 1000Hz, 

Will Figure 17 work same for the FSIGNAL 6KHz?

4. Is it possible to share the Spice model for LM1815 Chip?