This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432: How to change the ADC sampling time?

Part Number: AWRL6432

Hi Team,

We saw ADC sampling time is 300ns in GPADC parameters of datasheet 9.4.2.

Is it possible to change the value from 300ns to the others?

If yes, could you please tell us the method how to change?

Best regards,

Ito

  • Hey Ito-san,

    The ADC sampling time is determined by two parameters in the chirpComnCfg: DigOutputSampRate and NumOfAdcSamples. This can be calculated by taking the number of ADC samples and dividing by the sampling rate. Note: the DigOutputSampRate specifies the decimator to be used to determine the sampling rate (sampling rate = 100 MHz/DigOutputSampRate). For example, if DigOutputSampRate = 32 (Sampling Rate = 3.125 MHz) and NumOfAdcSamples = 128, then the sampling time is 40.96 ns (128/3.125 MHz).

    Regards,

    Kristien