Other Parts Discussed in Thread: AWR2944
Hello,
I only activated Tx0 and set the Phase Shifter as follows:
Profile id(0) - Phase Shifter Tx0(deg) : 0
Profile id(1) - Phase Shifter Tx0(deg) : 180
Profile id(2) - Phase Shifter Tx0(deg) : 0
Profile id(3) - Phase Shifter Tx0(deg): 180
I think Phase Shifter works like this:
Chirp0 - Profile id(0)
Chirp1 - Profile id(1)
Chirp2 - Profile id(2)
Chirp3 - Profile id(3)
Chirp4 - Profile id(0)
Chirp5 - Profile id(1)
Chirp6 - Profile id(2)
Chirp7 - Profile id(3)
...
Chirp127 - Profile id(2)
Chirp128 - Profile id(3)
Q1. Is this how Phase Shifter works?
And, the result of phase of 128 chirp through raw data is as shown in the attached picture.

Based on these results, it looks like Phase Shifter is not working properly.
Q2. Is there some problem? and how do I solve this problem?
Thanks,
Jason