This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL1432BOOST: Different Transmit power between Tx1 and Tx2

Part Number: IWRL1432BOOST

Hi team,

My customer has a problem when they tested IWRL1432BOOST. 

firstly, they download the example of level_sensing:

Secondly, they configured the channelCfg 1 1 0, which is T1. They found the signal is normal:

Then, they configured the channelCfg 1 2 0, which is T2. They found the signal is very little:

Do you know the reason?

BR,

Moon