This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843: ADC sampling rate

Part Number: AWR6843

Hi TI engineers,

I use sample code which project name is CPD with classification in toolbox 1.30.01.03.

I had some question about ADC sampling rate and the parameter name is called as digOutSampleRate in code.

Then i used the ADC data to simulate the sample code algorithm, and i set the sampling rate to 2.2MHz.

note that :  [ I attached the radar to the absorber to get the ADC data, which means no target.]

the figure as shown

when range bin from 63 to 64, it would occur discontinuities.

So, i increased the ADC sampling rate from 2.2MHz to 2.25MHz

and the issue seems fixed.

So, I want to know why it would be fix by increase the sampling rate.

and it is allow to set small change about ADC sampling rate (I mean 2.2Mhz -> 2.25Mhz , the samll change is 0.05Mhz, Does it work ?)

i want to ask this because the sampling rate usually set multiples of 2, or maybe i misunderstand.

thanks ! 

Sincerely,JcWu.