This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: How to modificate DCA1000 ethernet packet delay time

Part Number: DCA1000EVM

Hi expert,

     I use DCA1000 default  ethernet configuration data to caputure ADCdata,the default Ethernet delay is pre-programmed as 25 µs in both the FPGA and software,so  ethernet throughput varies up to 325 Mbps. 

Now I want to up to 515Mbps, but I cann't use mmwave studio GUI to change ethernet packet delay time. 

   There can be a other better way to change  it ,through  MMwave studio API  or change DCA1000 Firmware EEPROM?

tks!